Elliott Electric Supply Logo

FULL-LOAD CURRENT IN AMPERES SINGLE-PHASE ALTERNATING CURRENT MOTORS

HP 115V 200V 208V 230V
1/6 4.4 2.5 2.4 2.2
1/4 5.8 3.3 3.2 2.9
1/3 7.2 4.1 4 3.6
1/2 9.8 5.6 5.4 4.9
3/4 13.8 7.9 7.6 6.9
1 16 9.2 8.8 8
1 - 1/2 20 11.5 11 10
2 24 13.8 13.2 12
3 34 19.6 18.7 17
5 56 32.2 30.8 28
7-1/2 80 46 44 40
10 100 57.5 55 50

The voltages listed are rated motor voltages.
The listed currents are for system voltage ranges of 110 to 120 and 220 to 240.