POWER SURGES AND SPIKES
What are They?
Power surges are an increase in the voltage that powers electrical equipment. Surges often go unnoticed, often lasting only 1/20th of a second, but they are much
more common and destructive than you might think. According to recent studies, electrical equipment is constantly experiencing surges of varying power. Some of
them can be absorbed by a power supply while others can only be handled by a quality surge suppressor. The most destructive power surges will wipe out anything
that gets in their way!
Where do they come from?
In this power-hungry computer age, utility power systems are often pushed beyond their capacity, resulting in unstable, unreliable power for consumers. Overburdened
power grids can generate powerful surges as they switch between sources or generate "rolling surges" when power is momentarily disrupted. Local sources
can also generate surges (such as a motor starting, or a fuse blowing out).
What about Lightning?
Lightning can generate a spectacular surge along any conductive line to destroy everything in its path. NO MATTER WHAT MANUFACTURERS MAY CLAIM, NO SURGE SUPPRESSOR
IN THE WORLD CAN SURVIVE A DIRECT LIGHTENING STRIKE. However, with quality equipment the surge suppressor will take the hit - ending up melted - but the equipment
it protects will not be affected.
COMPARING AND CHOOSING THE RIGHT LEVEL OF PROTECTION
There are many rating systems that can measure surge protection:
Joule Ratings:
The bigger, the better! Joule ratings measure a surge suppressors ability to absorb surges.
- 200 Joules: Basic Protection
- 400 Joules: Good Protection
- 600+ Joules: Excellent Protection
Surge Amp Ratings:
Higher ratings offer more protection. Amp levels are another important factor in determining surge strength. Look for the highest amp protection levels available.
UL 1449 Voltage Let-Through Ratings:
Underwriter Laboratories tests each surge suppressor and rates them according to the amount of voltage they let-through to connected equipment. The lower the let-through
voltage, the better the surge suppressor is. UL established the 330 volt let-through as the benchmark because lower ratings added no real benefits to equipment
protection, while surge components, forced to work harder, failed prematurely. Be wary of manufacturers claiming lower let-through ratings.