Current Openings


← Back to Job Listings

An Elliott Electric Supply Store

Delivery Driver

Job Description:

Support warehouse operations by transporting materials over designated routes; ensuring safe operation of vehicles. Provide excellent customer service by making prompt and courteous deliveries of customer orders. Ensure that material loaded on the truck is as listed on the Ship Ticket and Delivery Manifest and is secured for safe transport from store to delivery location. Unload materials for customers at each delivery location in an orderly fashion while verifying that material being unloaded is correct based on the Ship Ticket. Perform daily detailed inspection of vehicle to ensure general maintenance and safety of vehicle. 

 

Requirements:

High school diploma or equivalent preferred. Must have a valid drivers license in state of residence with a minimum of three (3) driving history. Must have an acceptable motor vehicle record (MVR) with no type A violation; or no more than one (1) type B violation in the past three (3) years. Must be able to read, comprehend, write, perform calculations, input accurately, reason, and analyze. Function independently, completing a variety of tasks accurately and with close attention to detail in a team environment. 

Physical Requirements: Frequent driving is required. Visits to customers will expose the incumbent to all types of weather conditions. Must be aware of each customer’s environment and adhere to the proper safety regulations since there will be occasional exposure to events such as excessive noise and moving machinery. Frequent walk, bend, squat, climb, and kneel. Occasional pushing, pulling, and reaching Handling of objects and lifting of up to 50 pounds. Occasional lifting of up to 75 pounds.



Job Type: Full-Time Contact: Brian Circle (806)698-6329

Location: Lubbock, TX (110)

Apply For This Position