Current Openings


← Back to Job Listings

An Elliott Electric Supply Store

General Mechanic

Job Description:

Summary: Support warehouse operations by ensuring safe maintenance and operation of vehicles at the distribution center and stores in DFW Area.  Provide excellent customer service by making prompt repairs.

 

Responsibilities:

 

  • Maintain electric and propane forklifts, sitdown, reach, cherry picker, electric pallet jack, Raymond and Toyota preferred.

  • Forklift work includes hydraulics, grease, wearable items repair, parts changing, battery maintenance and install.

  • Maintain large commercial trucks including Ford F450s up to F750s and equivalent in other Makes and Models (Peterbilt, Isuzu, etc).

  • Truck maintenance includes oil changes, brakes, detailed Preventative Maintenance checklist, air filters, air leaks, change fan clutch, AC repairs, tires,

  • Maintain other equipment like wire machines, pallet jacks, pallet wrap machines, etc.

  • Drive in a careful, skillful, and defensive manner so material and vehicle are protected against damage.

  • Assist Safety Manager with any building maintenance and repair needs.

  • Assist in any and all warehouse duties on an as-needed basis.

  • Able to work some Saturdays.

  • Ability to weld would be beneficial.

  • ASC Certification is a plus.

Requirements:

Qualifications: High school diploma or equivalent preferred. Must have a valid Driver’s License in state of residence with a minimum of three (3) years driving history. Must have an acceptable motor vehicle record (MVR) with no type A violations; or no more than one (1) type B violation in the past three (3) years.  Have basic Mechanic hand tools.  Able to work on commercial trucks and forklifts including electric and propane lifts.  Good attitude, mechanically minded, with a desire to get the job done right and on time.  Must be able to read, comprehend, write, perform calculations, input accurately, reason, and analyze. Ability to function independently, completing a variety of tasks accurately, and with close attention to detail in a team environment.

 

Physical Requirements: Frequent driving is required. Visits to stores will expose the Mechanic to all types of weather conditions. Must be aware of each store’s environment and adhere to the proper safety regulations since there will be occasional exposure to events such as excessive noise and moving machinery. Frequent walk, bend, squat, climb, and kneel. Occasional pushing, pulling, and reaching Handling of objects and lifting of up to 50 pounds. Occasional lifting of up to 75 pounds. 

 



Job Type: Full-Time Contact: Tori Joseph (972)206-0016

Location: Farmers Branch, TX (DFW RDC - 34)

Apply For This Position