Current Openings


← Back to Job Listings

An Elliott Electric Supply Store

Delivery Driver

Job Description:

Support warehouse operations by transporting materials over designated routes; ensuring safe operation of vehicles.. Ensure that material loaded on the truck is as listed on the Ship Ticket and Delivery Manifest and is secured for safe transport from store to delivery location. Unload materials  at each delivery location in an orderly fashion while verifying that material being unloaded is correct based on the Ship Ticket. Will be delivering to satillete store locations after normal hours . Will put material in building and secure building before leaving each locations .  Perform daily detailed inspection of vehicle to ensure general maintenance and safety of vehicle. Hours will be 2:00pm to 11:00pm most days for a full time position or 4:30pm to 11:00pm for part time . The hours could be early morning , 4:30am till 2:00pm or part time 4:30sm till 11:00am Monday thru Friday or Tuesday thru Saturday .

Requirements:

High school diploma or equivalent preferred. Must have a valid driver’s license in state of residence with a minimum of three (3) driving history. Must have an acceptable motor vehicle record (MVR) with no type A violation; or no more than one (1) type B violation in the past three (3) years.  A Department of Transportation (DOT) physical examination will be conducted by a licensed "medical examiner. Must be able to read, comprehend, write, perform calculations, input accurately, reason, and analyze. Function independently, completing a variety of tasks accurately and with close attention to detail in a team environment.

 

Physical Requirements: Frequent driving is required. Visits to customers will expose the incumbent to all types of weather conditions. Must be aware of each customer’s environment and adhere to the proper safety regulations since there will be occasional exposure to events such as excessive noise and moving machinery. Frequent walk, bend, squat, climb, and kneel. Occasional pushing, pulling, and reaching Handling of objects and lifting of up to 50 pounds. Occasional lifting of up to 75 pounds. The ability to work in a constant state of alert and in a safe manner.



Job Type: Full-Time Contact: Richard Ogden (903)509-9882

Location: Tyler, TX (2)

Apply For This Position