Need Primary Control For Electrical Power?

The LoadCenter Controls Power Into and Around a Building.
Get Great Wholesale Prices At Elliott Electric Supply.

In most buildings, the LoadCenter is typically placed in out-of-the-way areas such as the basement, storage room, laundry room or garage. Why?

The LoadCenter needs to be placed at a location that will serve as the central point where power enters the building and is distributed. It is generally not located in an area that is open to tampering, but, on the same token, a LoadCenter should not be placed in an obscure, hard to reach area.

The LoadCenter is essentially the primary electrical brain for the building – it provides all the electrical power in and around the structure. The LoadCenter is often known by a variety of common names:

Sometimes this terminology is universally used to define a LoadCenter.

Essentially, the LoadCenter is a mounting enclosure for multiple electrical circuit breakers. The panel consists of two columns in most centers, while in some smaller centers, breakers are placed in just one column (e.g., in Great Britain).

Circuit breakers are used to de-energize electrical circuits when wiring is being serviced. A simple toggle switch indicates if the connected electrical outlets and the ensuing power supply are either on or off.

In North America, most Load Centers display all circuits as open when the door is open; a toggle of a different indicator color and applicable text indicates power to those has been terminated.

For top quality Load Centers, circuit breakers and electrical fuses, look to Elliott Electric Supply --- a premier electrical supplies distributor with over 800 employees and 100 locations in the southern US. Whatever the age of your house, we're sure to have the electrical components you need to keep it in tip-top condition.

With great pricing, extensive inventory, and fast delivery, you'll find no better wholesale electrical supply distributor online than Elliott Electric Supply. Shop online today!

Electric Motor Supplies, Electrical Boxes, Electrical Conduit, Electrical Meters , Electrical Wiring, Emergency Generator, Light Bulbs, Light fixtures, One Stop Electrical , Quality Emergency Lighting

Load Centers, Circuit Breakers and Electrical Fuses